cancel
Showing results for 
Search instead for 
Did you mean: 

Mistake in ST3232 datasheet

David Turner
Associate
Posted on January 24, 2017 at 01:05

In the

http://www.st.com/content/ccc/resource/technical/document/datasheet/group1/40/2c/7f/62/3a/3f/47/3c/CD00002253/files/CD00002253.pdf/jcr:content/translations/en.CD00002253.pdf

, the introduction text says:

The devices require only four small 0.1 mF standard external capacitors for operation from a 3 V supply.

However, Table 9 states the capacitance value as 0.1uF, a value 1000 smaller than 0.1mF.  Please could you confirm which of these is correct (I assume 0.1uF) and update the datasheet so the values agree?

David

1 REPLY 1
Tamas Novak
Associate III
Posted on March 18, 2017 at 17:49

It is surely 100nF. I've used it a number of times and worked well.