2017-01-23 4:05 PM
In the
, the introduction text says:The devices require only four small 0.1 mF standard external capacitors for operation from a 3 V supply.
However, Table 9 states the capacitance value as 0.1uF, a value 1000 smaller than 0.1mF. Please could you confirm which of these is correct (I assume 0.1uF) and update the datasheet so the values agree?
David
2017-03-18 9:49 AM
It is surely 100nF. I've used it a number of times and worked well.