2024-09-11 11:18 PM - last edited on 2024-09-12 04:25 AM by SofLit
我的 L9663 SPI 无法正常工作,我想通过寄存器读取L9663的设备ID,但接收回来都是0XFFFF。我现在使用的MCU是STM32F103C8T6,以下是我的计划,希望大佬们帮我看一下有没有问题。
2024-09-12 04:24 AM
Translation:
My L9663 SPI is not working properly. I want to read the device ID of L9663 through the register, but the received data is 0XFFFF. The MCU I am using now is STM32F103C8T6. The following is my plan. I hope you can help me check if there is any problem.
2024-11-14
12:29 AM
- last edited on
2024-11-14
04:27 AM
by
Maxime_MARCHETT
@mochensama , Hi, have you solved your problem? I designed the circuit with reference to spec, if you use PSI5-P mode, you shouldn't pull up BH1 of pin8, right? Also are you using 5V for VASSUP? I feel like it's usually with a higher voltage, right?
This post has been translated from Chinese to comply with the ST Community guidelines.
2025-01-18 11:20 PM
哥们你问题解决了吗,我是一个研一学生,如果可以的话你直接打我电话19153392385,咱一起讨论一下,我现在也遇到了这个问题。