2023-05-04 04:11 AM
2023-05-04 06:39 AM
Your're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-05-04 11:57 PM
Another question. Is there any programming tool available for STLINK-V3PWR? It seems that I also cannot connect with STM32CubeProg (does not support BLUENRG-LP) and RF-Flasher utility is only supporting UART.
2023-05-05 12:17 AM
Well, as already discussed, you will probably only get further with an ST-LINK/V2, possibly also ST-LINK/V2-1.
2023-05-05 12:21 AM
Ok. So there is no other possibility to use the STLINK-V3PWR for BLUENRG-LP at the moment?
2023-05-05 12:24 AM
Correct, as far as I am informed.
However, you can have it explicitly confirmed again in a personal ticket on the OLS online system.
2023-05-05 12:35 AM
Thanks.