2022-06-12 8:32 AM
I'm working on a new IOT device. I'm using your BLUENRG-232N device with STM32L496AGI6 microcontroller, and I'm using your STMicroelectronics.X-CUBE-BLE2 version 3.2.2 stack for the firmware and the application. but unfortunately the mcu goes into the Infinite_Loop: during the call of the MX_BlueNRG_2_Init function.
Find attached the demo_project and schematic.
Solved! Go to Solution.
2022-06-16 7:24 AM
Hello,
from your ioc I see you did not enable the EXTI line3 for the BlueNRG interrupt.
You should enable it as shown in the attached picture.
The EXTI line[15:10], also enabled in the picture, is used for the User Button that is configured in EXTI mode.
Please, let me know if this solve your issue.
BR
Silvio
2022-06-16 7:24 AM
Hello,
from your ioc I see you did not enable the EXTI line3 for the BlueNRG interrupt.
You should enable it as shown in the attached picture.
The EXTI line[15:10], also enabled in the picture, is used for the User Button that is configured in EXTI mode.
Please, let me know if this solve your issue.
BR
Silvio
2022-07-19 11:23 AM
It's working thank you so much