Hello,in the X-CUBE-BLE1 package V6.2.3 you can still find the BLE Peripheral Profile library and some sample application for the Nucleo-L476RG (they have been removed in release V6.2.4).You are not able to see them through the STM23CubeIDE since the...
Hi,when you create a project without one of the predefined sample applications, the MX_BlueNRG_MS_Init() and MX_BlueNRG_MS_Process() function are not generated by the STM32CubeMX.It is up to the user to write his/her own init and process functions in...
Hello,so far there is no X-CUBE package for the BlueNRG-LP.On st.com you can find the X-CUBE-BLE1 for the BlueNRG-M and the X-CUBE-BLE2 for the BlueNRG-2.The X-CUBE-BLEMGR pack is instead an abstraction layer providing APIs to manage the Bluetooth® L...
Hello Anil,you could have a look at the lib_gnss library (and at the sample applications) included in the X-CUBE-GNSS1 software pack available on st.com.BRSilvio