2021-10-04 7:41 PM
2021-10-04 11:54 PM
Welcome, @Ykuo.1, to the community!
Please note that the stack from TEConcept is not freely available and a license is required, as you can read in UM2232:
The version is fully featured but for a limited time (10000 minutes): after that, the system stops working and you
need a new free key license from TEConcept, with the hardware ID readable using their proprietary Control tool, a
graphical user interface (GUI) which enables communication with master unit and device.
Please also check the Getting Started - FAQs about IO-Link products.
If you don't want to write your own software from scratch, you should contact TEConcept as they are responsible for the IO-Link stack.
Regards
/Peter
2021-10-05 12:11 AM
Hi Peterm
If I don't have TEConcept tool , I need to use STM32CubeMX and STSW-IO-LINK(without stack) to create the Project by myself?
Or Reference Document "UM2232" page3.
Does ST provide the project ?
Thank you.
2021-10-05 1:43 AM
The schematics of STEVAL-IDP004V1 and STEVAL-IDP004V2 is essentially identical, so to start without stack you can try to use the project STSW-IO-LINK.
Regards
/Peter
2021-10-05 7:56 AM
I have download STSW-IO-LINK, but I don't know how to use STM32CubeMX to open the project.
Do you have any user manual or tutor document for STSW-IO-LINK ?
Why STM32CubeMX ST Board doesn't have the choice of STEVAL-IDP004V2?
2024-05-28 11:36 AM
Any update on this?