2015-03-27 4:23 AM
Hello,
Please, help me to clarify the following question: Can I set one specific channel for advertising (37 channel for example)? I have tried to usehci_le_set_advertising_parameters
function, but to no avail! Regards, Andrei Kukenov2015-03-27 5:26 PM
Are you sure that your call returns success? So something like this:
assert(BLE_STATUS_SUCCESS == hci_le_set_advertising_parameters( ADV_INTERVAL_LOWEST_CONN, ADV_INTERVAL_LOWEST_CONN, ADV_IND, PUBLIC_ADDR, PUBLIC_ADDR, advData.brdAddr, ADV_CH_37, NO_WHITE_LIST_USE)); AND, that subsequently you only use hci to update advertising data and turn advertising on and off? I think that the higher level ACI start advertising call blows away anything you've setup with hci calls.2015-03-30 12:09 AM
and
I do not have
any
idea
why
,
possibly
incorrect
sequence
. And, yes, I think just use hci to update advertising. Regards, Andrei Kukenov2015-04-02 2:07 AM
Hi,
The the stack firmware version 6.4 contains only a subset of HCI commands, in particular the command HCI_LE_SET_ADVERTISING_PARAMETERS has been replaced by ACI_GAP_SET_DISCOVERABLE paramaeters. for futher details, please see the ''BlueNRG, BlueNRG-MS Bluetooth LE Stacks Release Notes''. Regards, Graziella2015-04-02 2:16 AM
Hi,
If you want only the HCI command, you can load the fw images: - bluenrg_6_4_Mode_2-16MHz-XO32K_HCI.img,- bluenrg_6_4_Mode_2-32MHz-XO32K_HCI.img'' These BlueNRG stack v6.4 binary images supporting only the HCI APIs (no GAP APIs) are provided. Regards, Graziella
Hi,
The the stack firmware version 6.4 contains only a subset of HCI commands, in particular the command HCI_LE_SET_ADVERTISING_PARAMETERS has been replaced by ACI_GAP_SET_DISCOVERABLE paramaeters. for futher details, please see the ''BlueNRG, BlueNRG-MS Bluetooth LE Stacks Release Notes''. Regards, Graziella2015-04-02 5:16 AM
2015-04-02 4:33 PM
Dear Graziella / ST:
What if an application is depending on BOTH using ACI commands and some HCI commands?! Why did ST remove such a valuable command as hci_le_set_advertising_parameters()? The reason that command is so valuable is that you surely know that when using the ACI_GAP_SET_DISCOVERABLE command, the BlueNRG firmware just automatically adds onto the advertising data 2 additional items that are never explicitly asked for from the App driving the BlueNRG. Do you know of a work-around for this (i.e. how to prevent the BlueNRG from automatically adding those 2 extra items to the advertising data)? Thanks for any hints.2015-04-03 12:36 AM
Hi,
instead to use the command hci_le_set_advertising_parameters(), as you said, you can use the command ACI_GAP_SET_DISCOVERABLE and the command ACI_GAP_UPDATE_ADV_DATA to update the Advertising Data.
For futher details, you can see the example of Beacon application (Fw code under forlder ..\Projects\Project\BLE_Beacon or script under folder ..Application\scripts\BLE_Beacon).
Regards,
Graziella MarcheseDear Graziella / ST:
What if an application is depending on BOTH using ACI commands and some HCI commands?! Why did ST remove such a valuable command as hci_le_set_advertising_parameters()? The reason that command is so valuable is that you surely know that when using the ACI_GAP_SET_DISCOVERABLE command, the BlueNRG firmware just automatically adds onto the advertising data 2 additional items that are never explicitly asked for from the App driving the BlueNRG. Do you know of a work-around for this (i.e. how to prevent the BlueNRG from automatically adding those 2 extra items to the advertising data)? Thanks for any hints.