cancel
Showing results for 
Search instead for 
Did you mean: 

Changing advertising data STM32WPAN

KlemenPfce
Associate III

Hello,

 

I have custom PCB with STM32WB5MM module configured as beacon. I am successfully advertising configured data.

I have configured a task in sequencer (the task gets executed, checked with debugging). When I leave task empty, the BLE advertises, but when I add function to update adv data, the advertising stops.

Configured data manufacturer specific data: 100000000000000090 

"New" configured data manufacturer specific data: 100000000011111190 

 

My function:

 

 

void MyTask(void){

	uint8_t alt_AdvData[28] =
	{
	  2, AD_TYPE_TX_POWER_LEVEL, 0 /* -0.15dBm */, /* Transmission Power */
	  7, AD_TYPE_COMPLETE_LOCAL_NAME, 'F', 'P', '0', '0', '0', '1',  /* Complete name */
	  3, AD_TYPE_16_BIT_SERV_UUID_CMPLT_LIST, 0x0D, 0x18,
	  12, AD_TYPE_MANUFACTURER_SPECIFIC_DATA, 0x30, 0x00, 0x10 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x11 /*  */, 0x11 /*  */, 0x11 /*  */, 0x90 /*  */,
	};
	aci_gap_update_adv_data(sizeof(alt_AdvData), (uint8_t*) alt_AdvData);
}

 

 

In "alt_AdvData" I currently store "new data" to advertise, at later point they will be dynamically changed.

1 REPLY 1
STTwo-32
ST Employee

Hello @KlemenPfce 

Have you tested that the task you are mentioning is working correctly. Could you please give more details.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.