2015-10-27 07:40 AM
Hi,
I would like to communicate with the LCD display. How can i connect the display?. Are there any separate pins dedicated for LCD data bits or i can connect to any GPIO pin. Here i would like to send the serial data (SPI) of a 3-axis sensor to LCD display.2015-10-29 07:29 AM
Sorry dear customer,
but the Low Power RF Solutions forum is exclusively dedicated to Bluetooth Low Energy and Spirit1 devices, thus here you cannot find the right support you deserve.Regards,
Low Power RF Solutions support teamHi,
I would like to communicate with the LCD display. How can i connect the display?. Are there any separate pins dedicated for LCD data bits or i can connect to any GPIO pin. Here i would like to send the serial data (SPI) of a 3-axis sensor to LCD display.2016-01-06 10:00 AM
Hi,
I use an X-NUCLEO-IDB05A1 on NUCLEO-L053R8; i want write on a terminal (for example using Tera Term) with ''printf'' for debugging my application. What can I do? If I use a ''printf'' in the Tera Term Terminal don't appear anything. I don't know if is a Tera Term's setting problem or everything in my application.Thanks2016-01-13 02:49 AM
Dear Customer,
after you connect your board to PC, using TeraTerm you have: - By Setup -> Serial Port, set Baud Rate to 115200 - to create a New Nonnection and open the COM port related to your device. Regards, GM2016-01-14 10:13 AM
Hi, I want use an X-NUCLEO-IDB05A1 on (STEVAL-IDB002V1) RF MOTHERBOARD (vers 3.0). How do you connect them?
2016-01-15 03:16 AM
Dear Customer,
the X-NUCLEO-IDB05A1 is an expansion board of the STM32 Nucleo boards, therefore, you can not mount it on a on STEVAL-IDB002V1 RF MOTHERBOARD.
For futher details about the expansion board X-NUCLEO-IDB05A1, please see the following link:
http://www.st.com/web/catalog/tools/FM146/CL2167/SC2006/LN1988/PF262191?s_searchtype=partnumber
Regards,
GM
Hi, I want use an X-NUCLEO-IDB05A1 on (STEVAL-IDB002V1) RF MOTHERBOARD (vers 3.0). How do you connect them?
2016-01-19 06:27 AM