2015-01-09 9:46 AM
Hi,
I'm trying to customize the advertising packet, but it's unsuccessful so far.
I use STEVAL-IDB002V1
BlueNRG HW v3.0
BlueNRG FW v6.4
Motherboard FW v1.4
Since the command ACI_GAP_SET_DISCOVARABLE doesn't give much options I've tried to use HCI_LE_SET_ADVERTISING_PARAMETERS , HCI_LE_Set_Advertizing_Data, HCI_LE_SET_ADVERTISE_ENABLE.
The response to HCI_LE_SET_ADVERTISING_PARAMETERS and HCI_LE_SET_ADVERTISE_ENABLE is Unknown HCI Command.
Are these supported commands?
Is there any other way to customize the advertising and scan packet?
Thanks
2015-01-09 9:56 AM
Using the BlueNRG X-NUCLEO-IDB04A1 running FW 6.3, I have been able to successfully control the advertising data to whatever I want with this:
uint8_t advData[31] = { the specific bytes I want, using the advertising data format of ''LENGTH-TYPE-DATA'', so e.g. 0x06, 0xFF, 'H', 'e', 'l', 'l', 'o' }; rtrnVal = hci_le_set_advertising_data(sizeof(advData), (uint8_t const*)&advData); Note that I also use this to start advertising: rtrnVal = hci_le_set_advertise_enable(true);2015-01-09 1:08 PM
I programmed the bluenrg_6_4_Mode_2-16MHz-XO32K_HCI.img and now the HCI_LE_SET_ADVERTISING_PARAMETERS and HCI_LE_SET_ADVERTISE_ENABLE complete successfully, but during scanning the software doesn't show any data. It shows only the BLE address.
First I run the Initialization script to start the GAT and GAPP and then
send HCI_LE_SET_ADVERTISING_PARAMETERS (ADV_IND, advertise on all channels..)
send HCI_LE_SET_ADVERTISING_DATA
Parameter Total Length 0x20
Advertising_Data_Length 0x0F
Advertising_Data 0x0201060808426C75654D4641020AFE00000000000000000000000000000000
send HCI_LE_SET_ADVERTISE_ENABLE
For scanning I use nRF Master Control on my tablet and it shows only the bluetooth address.
Do I need to setup something else?
2015-01-21 4:09 AM
Hi Dimitar,
To customize the Advertising packet, you should use the command ACI_GAP_UPDATE_ADV_DATA where the advData has to be formatted as specified in Bluetooth specification (volume 3, Part C, 11).
Instead, If you use the HCI command, you don't send the commands GATT_init and GAP_init.Regards,
GraziellaHi,
I'm trying to customize the advertising packet, but it's unsuccessful so far.
I use STEVAL-IDB002V1
BlueNRG HW v3.0
BlueNRG FW v6.4
Motherboard FW v1.4
Since the command ACI_GAP_SET_DISCOVARABLE doesn't give much options I've tried to use HCI_LE_SET_ADVERTISING_PARAMETERS , HCI_LE_Set_Advertizing_Data, HCI_LE_SET_ADVERTISE_ENABLE.
The response to HCI_LE_SET_ADVERTISING_PARAMETERS and HCI_LE_SET_ADVERTISE_ENABLE is Unknown HCI Command.
Are these supported commands?
Is there any other way to customize the advertising and scan packet?
Thanks
2015-03-24 2:12 AM
Hello, Guys
Dimitar, you can use the following sample http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00099259.pdf page 50 This example work fine on my board (fw 6.4) If you need additional information, please, feel free to ack me. Regards, Andrei Kukenov2015-09-15 2:36 AM
Hi,
I'm trying to customize the advertising packet, but it's unsuccessful so far.
I use STEVAL-IDB002V1
I followed the following information of BlueNRG Beacon demonstration application:
<<
The BLE Beacon device uses the GAP ACI command to enter non-connectable mode as
follows:
aci_gap_set_discoverable(ADV_NONCONN_IND, 160, 160, PUBLIC_ADDR,
NO_WHITE_LIST_USE,0, NULL, 0, NULL, 0, 0);
In order to advertise the specific selected manufacturer data, the BLE Beacon application
uses the following GAP ACIs:
/* Remove TX power level field from the advertising data: it is necessary to have enough
space for the beacon manufacturing data */
ret = aci_gap_delete_ad_type(AD_TYPE_TX_POWER_LEVEL);
/* Define the beacon manufacturing payload */
const uint8_t manuf_data[] = {26, AD_TYPE_MANUFACTURER_SPECIFIC_DATA,
0x30, 0x00, //Company identifier code (Default is 0x0030 - STMicroelectronics)
0x02, // ID
0x15, //Length of the remaining payload
0xE2, 0x0A, 0x39, 0xF4, 0x73, 0xF5, 0x4B, 0xC4, //Location UUID
0xA1, 0x2F, 0x17, 0xD1, 0xAD, 0x07, 0xA9, 0x61,
0x00, 0x00, // Major number
0x00, 0x00, // Minor number
0xC8 //2's complement of the Tx power (-56dB)};
};
/* Set the beacon manufacturing data on the advertising packet */
ret = aci_gap_update_adv_data(27, manuf_data);
>>
Unfortunately, the receiver does not detect event so I don't know if the advertisement is received.
What's the matter?
Is there any other way to send the advertising and detect advertisement packet on the receiver?
Thanks
2015-09-17 7:25 AM
Hi Luca,
Which stack fw version are you using?
Are you yuo download the latest version of GUI DK from ? Could you give us major information? for example who is the receiver and how is it configured?Regards,
Graziella MarcheseHi,
I'm trying to customize the advertising packet, but it's unsuccessful so far.
I use STEVAL-IDB002V1
I followed the following information of BlueNRG Beacon demonstration application:
<<
The BLE Beacon device uses the GAP ACI command to enter non-connectable mode as
follows:
aci_gap_set_discoverable(ADV_NONCONN_IND, 160, 160, PUBLIC_ADDR,
NO_WHITE_LIST_USE,0, NULL, 0, NULL, 0, 0);
In order to advertise the specific selected manufacturer data, the BLE Beacon application
uses the following GAP ACIs:
/* Remove TX power level field from the advertising data: it is necessary to have enough
space for the beacon manufacturing data */
ret = aci_gap_delete_ad_type(AD_TYPE_TX_POWER_LEVEL);
/* Define the beacon manufacturing payload */
const uint8_t manuf_data[] = {26, AD_TYPE_MANUFACTURER_SPECIFIC_DATA,
0x30, 0x00, //Company identifier code (Default is 0x0030 - STMicroelectronics)
0x02, // ID
0x15, //Length of the remaining payload
0xE2, 0x0A, 0x39, 0xF4, 0x73, 0xF5, 0x4B, 0xC4, //Location UUID
0xA1, 0x2F, 0x17, 0xD1, 0xAD, 0x07, 0xA9, 0x61,
0x00, 0x00, // Major number
0x00, 0x00, // Minor number
0xC8 //2's complement of the Tx power (-56dB)};
};
/* Set the beacon manufacturing data on the advertising packet */
ret = aci_gap_update_adv_data(27, manuf_data);
>>
Unfortunately, the receiver does not detect event so I don't know if the advertisement is received.
What's the matter?
Is there any other way to send the advertising and detect advertisement packet on the receiver?
Thanks
2015-11-06 9:06 AM
2015-11-06 9:10 AM
2015-11-09 12:18 AM
Dear Customer,
Evt_Blue_Gap_Device_Found event is not anymore returned from BlueNRG-MS stack v7.1 when a device is found during a discovery procedure, the LE_Advertising_Report event is returned from BlueNRG-MS stack v7.1 when a device is found durign a device discovery procedure. (Please see the release Note for futher information). Regards, GM