2020-12-04 08:59 AM
Hello,
I have X-NUCLEO-BNRG2A1 module, running the BLE2 sample application with some modification. I mannage to connect to the module with my Windows PC.
I would like to send data to it using a COM Port. But the Bluetooth is not seens as a COM port. I could note change it in windows option.
It seems that device add to "show" the "Standard Serial over Bluetooth" capabilities.
Any one knows how to add it? I could not find such a function in the SampleApplication and BLE stack.
Thank you
2020-12-09 01:30 AM
Hello,
Is there anybody to add "Standard Serial over Bluetooth link" to an STM32 Device with a X-NUCLEO-BNRG2A1?
I still canot add COM Port when connecting to my bluetooth decive
Antoine