2021-03-21 07:09 AM
Hi Everyone
I can't achieve the 500kbps using the following setup, which according to the S2LP datasheet is possible:
HW Setup used for the test:
main boards;
Radio boards:
FW loaded into Main boards:
The boards are placed barely 10cm one from other
The first test using the default init setting of S2LP DK SW is successful, 10 of 10 packets from Tx board reach the Rx board using the "Transmission Test" menu
As I switch from default datarate to 125 ksps datarate in both boards with the following radio settings:
The receiver is not able to receive any of the packets transmitted at 125ksps by the Tx board.
Did anyione experienced the same problem with this or similar test setup??
Thanks in advance!