2020-02-19 3:06 AM
Hi,
I want to use an USB device in order to load the .elf file via USB on STM32F746.
How can I do this?
Best Regards
2020-02-25 1:28 AM
Any ideas ?
2022-01-02 4:19 AM
this convert .BIN to DFU
use DfuSe --> "dfu file manager"
C:\Program Files (x86)\STMicroelectronics\Software\DfuSe v3.0.6\Bin\DfuFileMgr.exe
option one
multiBin
select file.
add to list
ok
Generate
2022-01-03 4:02 AM
in my case STM32F207IGT
compiler project in release mode. --> .bin
"Dfu file manager"
08000000 (in map file show adress: FLASH 0x0000000008000000 0x0000000000100000 xr
DF11 produc ID (in DfuseDemo show show this information)
2200 version (in DfuseDemo show show this information)
DfuSeDemo --> in case STM32F207IGT: on the user board it only changes position SW boot0 [boot/Run]