2022-07-17 8:51 PM
I am trying to edit the BLE Sensor Demo app for STM32 micro and BLUENRG-M0 module (using Nucleo boards).
I want to advertise one service in the advertising packet. When I make the call to aci_gap_set_discoverable() I get a response of BLE_STATUS_INVALID_PARAMS( 66 dec ) . The only change I made to the example source code is to add in the HW service UUID as used in the sample code.
void Set_DeviceConnectable(void)
{
uint8_t ret;
const char local_name[] = {AD_TYPE_COMPLETE_LOCAL_NAME,SENSOR_DEMO_NAME};
uint8_t svc_uuid[] = { 0x07,0x00,0x00,0x00,0x00,0x00,0x01,0x11,0xe1,0x9a,0xb4,0x00,0x02,0xa5,0xd5,0xc5,0x1b};
uint8_t manuf_data[] = {
2,0x0A,0x00, /* 0 dBm */ // Trasmission Power
8,0x09,SENSOR_DEMO_NAME, // Complete Name
11,0xFF,0xFF, /* SKD version */
0x52,
0x41,
0x4c,
bdaddr[5], /* BLE MAC start -MSB first- */
bdaddr[4],
bdaddr[3],
bdaddr[2],
bdaddr[1],
bdaddr[0] /* BLE MAC stop */
};
//manuf_data[18] |= 0x01; /* Sensor Fusion */
//COPY_HW_SENS_W2ST_SERVICE_UUID(svc_uuid);
hci_le_set_scan_resp_data(0, NULL);
PRINT_INFO("Set General Discoverable Mode.\n");
ret = aci_gap_set_discoverable(ADV_DATA_TYPE,
(ADV_INTERVAL_MIN_MS*1000)/625,(ADV_INTERVAL_MAX_MS*1000)/625,
STATIC_RANDOM_ADDR, NO_WHITE_LIST_USE,
//sizeof(local_name), local_name, 0, NULL, 0, 0);
sizeof(local_name), local_name, sizeof(svc_uuid), svc_uuid, 0, 0);
aci_gap_update_adv_data(sizeof(manuf_data), manuf_data);
if(ret != BLE_STATUS_SUCCESS)
{
PRINT_ERR("aci_gap_set_discoverable() failed: 0x%02x\r\n", ret);
}
else
{
PRINT_INFO("aci_gap_set_discoverable() --> SUCCESS\r\n");
}
}
Inside the aci_gap_set_discoverable() the code successfully passes the buffer overrun check so the error value of BLE_STATUS_INVALID_PARAMS comes after calling the hci_send_req(). Something is wrong is how I am formatting the service uuid and I can't find any example code on how to do this from STM.
Thanks
2022-07-21 3:23 AM
Hi @MD'Si.1 ,
I would advise to start from "SensorDemo_BLESensor-App" code example availabel in X-CUBE-BLE1 package.
You will see examples of UUID format for sevrice/charateristics. Always take care of Endianess with BLE<
As well in your code example, UUID looks to be 17bytes .. UUID are 128 bits.
Regards,
Sebastien.
2022-07-21 11:02 AM
@Sebastien DENOUAL Thanks for the suggestion. I am using the example you suggested and I still see incorrect behavior. The uuid I am trying to add to the advertising packet is 000000000001-11e1-9ab4-0002a5d5c51b which is the one used in the BLE Sensor APP example code (HW service)
I don't think the aci_gap_set_discoverable() has been verified with a uuid 128 list. The function or some underlying call does not account for the AD Type to be inserted just like the local_name variable. I tried 3 things below and each time the advertising packed was either nor formed or formed incorrectly.
Code for point number 1
void Set_DeviceConnectable(void)
{
uint8_t ret;
uint8_t local_name[] = {AD_TYPE_COMPLETE_LOCAL_NAME,SENSOR_DEMO_NAME};
uint8_t svc_uuid_list[] = {0x1b,0xc5,0xd5,0xa5,0x02,0x00,0xb4,0x9a,0xe1,0x11,0x01,0x00,0x00,0x00,0x00,0x00};
//uint8_t svc_uuid_list[] = {AD_TYPE_128_BIT_SERV_UUID,0x00,0x00,0x00,0x00,0x01,0x11,0xe1,0x9a,0xb4,0x00,0x02,0xa5,0xd5,0xc5,0x1b};
uint8_t manuf_data[5] = {
//2,0x0A,0x00, /* 0 dBm */ // Trasmission Power
//7,0x09,SENSOR_DEMO_NAME, // Complete Name
//17,0x06,0x1b,0xc5,0xd5,0xa5,0x02,0x00,0xb4,0x9a,0xe1,0x11,0x01,0x00,0x00,0x00,0x00,0x0,
4,0xff,0x52,0x41,0x4c
};
//manuf_data[18] |= 0x01; /* Sensor Fusion */
hci_le_set_scan_response_data(0,NULL);
PRINT_DBG("Set General Discoverable Mode.\r\n");
ret = aci_gap_set_discoverable(ADV_DATA_TYPE,
ADV_INTERV_MIN, ADV_INTERV_MAX,
PUBLIC_ADDR,
NO_WHITE_LIST_USE,
//sizeof(local_name), local_name, 0, NULL, 0, 0);
sizeof(local_name), local_name, 16, svc_uuid_list, 0, 0);
aci_gap_update_adv_data(5, manuf_data);
if(ret != BLE_STATUS_SUCCESS) {
PRINT_DBG("aci_gap_set_discoverable() failed: 0x%02x\r\n", ret);
}
else {
PRINT_DBG("aci_gap_set_discoverable() --> SUCCESS\r\n");
}
}
Code for point number 2
void Set_DeviceConnectable(void)
{
uint8_t ret;
uint8_t local_name[] = {AD_TYPE_COMPLETE_LOCAL_NAME,SENSOR_DEMO_NAME};
uint8_t svc_uuid_list[] = {AD_TYPE_128_BIT_SERV_UUID,0x1b,0xc5,0xd5,0xa5,0x02,0x00,0xb4,0x9a,0xe1,0x11,0x01,0x00,0x00,0x00,0x00,0x00};
//uint8_t svc_uuid_list[] = {AD_TYPE_128_BIT_SERV_UUID,0x00,0x00,0x00,0x00,0x01,0x11,0xe1,0x9a,0xb4,0x00,0x02,0xa5,0xd5,0xc5,0x1b};
uint8_t manuf_data[5] = {
//2,0x0A,0x00, /* 0 dBm */ // Trasmission Power
//7,0x09,SENSOR_DEMO_NAME, // Complete Name
//17,0x06,0x1b,0xc5,0xd5,0xa5,0x02,0x00,0xb4,0x9a,0xe1,0x11,0x01,0x00,0x00,0x00,0x00,0x0,
4,0xff,0x52,0x41,0x4c
};
//manuf_data[18] |= 0x01; /* Sensor Fusion */
hci_le_set_scan_response_data(0,NULL);
PRINT_DBG("Set General Discoverable Mode.\r\n");
ret = aci_gap_set_discoverable(ADV_DATA_TYPE,
ADV_INTERV_MIN, ADV_INTERV_MAX,
PUBLIC_ADDR,
NO_WHITE_LIST_USE,
//sizeof(local_name), local_name, 0, NULL, 0, 0);
sizeof(local_name), local_name, 17, svc_uuid_list, 0, 0);
aci_gap_update_adv_data(5, manuf_data);
if(ret != BLE_STATUS_SUCCESS) {
PRINT_DBG("aci_gap_set_discoverable() failed: 0x%02x\r\n", ret);
}
else {
PRINT_DBG("aci_gap_set_discoverable() --> SUCCESS\r\n");
}
}
Code for point number 3.
void Set_DeviceConnectable(void)
{
uint8_t ret;
uint8_t local_name[] = {AD_TYPE_COMPLETE_LOCAL_NAME,SENSOR_DEMO_NAME};
uint8_t svc_uuid_list[] = {AD_TYPE_128_BIT_SERV_UUID,0x1b,0xc5,0xd5,0xa5,0x02,0x00,0xb4,0x9a,0xe1,0x11,0x01,0x00,0x00,0x00,0x00};
//uint8_t svc_uuid_list[] = {AD_TYPE_128_BIT_SERV_UUID,0x00,0x00,0x00,0x00,0x01,0x11,0xe1,0x9a,0xb4,0x00,0x02,0xa5,0xd5,0xc5,0x1b};
uint8_t manuf_data[5] = {
//2,0x0A,0x00, /* 0 dBm */ // Trasmission Power
//7,0x09,SENSOR_DEMO_NAME, // Complete Name
//17,0x06,0x1b,0xc5,0xd5,0xa5,0x02,0x00,0xb4,0x9a,0xe1,0x11,0x01,0x00,0x00,0x00,0x00,0x0,
4,0xff,0x52,0x41,0x4c
};
//manuf_data[18] |= 0x01; /* Sensor Fusion */
hci_le_set_scan_response_data(0,NULL);
PRINT_DBG("Set General Discoverable Mode.\r\n");
ret = aci_gap_set_discoverable(ADV_DATA_TYPE,
ADV_INTERV_MIN, ADV_INTERV_MAX,
PUBLIC_ADDR,
NO_WHITE_LIST_USE,
//sizeof(local_name), local_name, 0, NULL, 0, 0);
sizeof(local_name), local_name, 16, svc_uuid_list, 0, 0);
aci_gap_update_adv_data(5, manuf_data);
if(ret != BLE_STATUS_SUCCESS) {
PRINT_DBG("aci_gap_set_discoverable() failed: 0x%02x\r\n", ret);
}
else {
PRINT_DBG("aci_gap_set_discoverable() --> SUCCESS\r\n");
}
}
2022-07-21 9:19 PM
@Sebastien DENOUAL I was able to get the service list to work with a 128 bit uuid and I did have to declare 17 octets for the function to work. To make it work I had to reduce the size of the local advertised name by about half.
Is there a way to increase the size so I can have a longer name and a 128 bit UUID. I have seen other bluetooth 4 chipsets support this feature so is it a configuration issue?
#define SENSOR_DEMO_NAME 'B','l','u','e' //,'N','R','G'
void Set_DeviceConnectable(void)
{
uint8_t ret;
uint8_t local_name[] = {AD_TYPE_COMPLETE_LOCAL_NAME,SENSOR_DEMO_NAME};
uint8_t svc_uuid_list[] = {AD_TYPE_128_BIT_SERV_UUID,0x1b,0xc5,0xd5,0xa5,0x02,0x00,0xb4,0x9a,0xe1,0x11,0x01,0x00,0x00,0x00,0x00,0x00};
uint8_t manuf_data[23] = {
//2,0x0A,0x00, /* 0 dBm */ // Trasmission Power
//7,0x09,SENSOR_DEMO_NAME, // Complete Name
//0x11,0x06,0x1b,0xc5,0xd5,0xa5,0x02,0x00,0xb4,0x9a,0xe1,0x11,0x01,0x00,0x00,0x00,0x00,0x0,
4,0xff,0x52,0x41,0x4c
};
//manuf_data[18] |= 0x01; /* Sensor Fusion */
hci_le_set_scan_response_data(0,NULL);
PRINT_DBG("Set General Discoverable Mode.\r\n");
ret = aci_gap_set_discoverable(ADV_DATA_TYPE,
ADV_INTERV_MIN, ADV_INTERV_MAX,
PUBLIC_ADDR,
NO_WHITE_LIST_USE,
//sizeof(local_name), local_name, 0, NULL, 0, 0);
sizeof(local_name), local_name, 17, svc_uuid_list, 0, 0);
aci_gap_update_adv_data(23, manuf_data);
if(ret != BLE_STATUS_SUCCESS) {
PRINT_DBG("aci_gap_set_discoverable() failed: 0x%02x\r\n", ret);
}
else {
PRINT_DBG("aci_gap_set_discoverable() --> SUCCESS\r\n");
}
}