2019-01-28 4:29 AM
hi,
i am searching for the information about the data rate and TX power value in Mesh code where can i find this information ?
In datasheet the air data rate is about 1 Mbit/s is this data rate the same like for the BlueNRG-1 Mesh ?
Thank you
2019-02-05 5:37 AM
Did you review the function Appli_BleSetTxPowerCb for setting the Tx Power ?
The BLE-Mesh is for low data rate applications. You can consider 8bytes application data being transferred per 20ms of advertisement interval. Then the size of Mesh will define the total application throughput