cancel
Showing results for 
Search instead for 
Did you mean: 

Currently we are using KS8721CL of MFR : Microchip and we are looking for an alternate part , Could you suggest an alternate part

MM.25
Associate II
 
4 REPLIES 4
Peter BENSCH
ST Employee

Welcome, @MM.25​, to the community!

The KS8721CL is or was a PHY for 10BASE-T, 100BASE-TX and 100BASEFX, which STMicroelectronics does not have in its portfolio. However, maybe one of the users in the community has a recommendation for you.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MM.25
Associate II

Thank you peter

Peter BENSCH
ST Employee

You're welcome!

If the problem is solved at some point, please mark this thread as answered by selecting Select as best for the relevant answer, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Piranha
Chief II

You are asking for alternates, but have not named a single requirement and have not even told what exactly you mean by "alternate". With such amount of information I can recommend DP83561.