2018-08-13 05:37 AM
If I changed the definition LS_SOURCE=LS_SOURCE_INTERNAL_RO, the procedure DeviceConfiguration() stopped in line "while(CKGEN_BLE->CLK32K_IT == 0);"
It seems that the internal generator 32 kHz does not work.
How I can to turn on generator 32 kHz.
2018-08-14 02:05 AM
Hi MicroLine,
I've just tested again and
It works for me normally.
Could you please try STEVAL-IDB007V1 or V2 with the latest DK (v3.0.0)
and modify project Options | C/C++ Compiler | Defined symbols, then set
LS_SOURCE=LS_SOURCE_INTERNAL_RO
Thank you.
Best Regards,
Winfred