cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use STLINK-V3 SWD for BlueNRG debug?

plumyay
Associate

Hi,

I'm trying to use STLINK-V3 MB1440B for BlueNRG2 debug. I'm connecting the SWD connector on STLINK to JTAG connector on BlueNRG development board. The BlueNRG-1_2 flasher shows "Waiting device to read ->" and stucks there when I tried to read the device memory. Pins I'm using are SWTDIO, SWTCLK, RESETN, GND, and VCC(3.3V). Is this correct way for SWD port to debug? Why BlueNRG flasher cannot detect my STLink?

Thanks.

0 REPLIES 0