cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-MS and firmware v7.1

charles23
Associate III
Posted on April 20, 2015 at 15:40

The BlueNRG DK 1.7.0 includes firmware images (V7.1) and API documentation for ''BlueNRG-MS devices.

Can you please explain the differences between BlueNRG and BlueNRG-MS? Other than support for Bluetooth 4.1 in BlueNRG-MS, it is difficult to see any significant differences. Are these the same hardware with different firmware, or different hardware?

Can the firmware in a BlueNRG chip be upgraded from v6.4 to v7.1? Are there advantages in doing so (for example, bug fixes in the later firmware).
5 REPLIES 5
Posted on May 11, 2015 at 11:46

Hi Palmer,

The BlueNRG and BlueNRG-MS have a different firmware on a different hardware. Therefore, you cannot upgrade a BlueNRG device with fw v.7.1.

The BlueNRG-MS is a very low power Bluetooth low energy (BLE) single-mode network processor, compliant with Bluetooth specification v4.1, and it supports multiple roles simultaneously.

For further information you can see the product specification that you can find at the following link:

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00141263.pdf

Regards,

GM

The BlueNRG DK 1.7.0 includes firmware images (V7.1) and API documentation for ''BlueNRG-MS devices.

Can you please explain the differences between BlueNRG and BlueNRG-MS? Other than support for Bluetooth 4.1 in BlueNRG-MS, it is difficult to see any significant differences. Are these the same hardware with different firmware, or different hardware?

Can the firmware in a BlueNRG chip be upgraded from v6.4 to v7.1? Are there advantages in doing so (for example, bug fixes in the later firmware).
peterpeter9161
Associate II
Posted on October 15, 2015 at 20:13

Hi Graziella,

in order BlueNRG-MS as Maste and keep connection with 3 BlueNRG-MS  slaves, what is the stack mode IFR? Do I have to program also BLE stack?

thanks,

Jose

Posted on October 19, 2015 at 11:15

You should set Stack Mode 3.

regards,

GM

peterpeter9161
Associate II
Posted on October 20, 2015 at 13:15

Hi Graziella,

Where I can find the default values of IFR for BlueNRG-MS?

Thanks, Jose

Posted on October 22, 2015 at 16:10

Dear Customer,

In the GUI DK, you can see the window Tools-> BlueNRG IFR window.

Regards,

GM