cancel
Showing results for 
Search instead for 
Did you mean: 

54AC164245 and 5962R9858008VZC

rpmiller
Visitor

Hi I'm using this device in a space design.  I just want to clarify the voltage requirements.  In all cases, I have Vdd1 >= Vdd2, as specified.  However, I'm using the device in these configurations and I want to confirm that the voltage levels are valid (it appears so from the datasheet but it's a little confusing):

Vdd1=5.0V, Vdd2=5.0V

Vdd1=3.3V, Vdd2=3.3V

Vdd1=5.0V, Vdd2=3.3V

Vdd1=5.0V, Vdd2=2.5V

Vdd1=3.3V, Vdd2=2.5V

Also, is there any requirement for the power connections for the 2 halves of the part.  For instance, I have one part with Vdd1-1=5.0V, Vdd2-1=3.3V  and Vdd1-2=3.3V, Vdd2-2=2.5V.

Thanks for your time,

Ryan Miller

Chief Engineer, Digital System

University of Michigan

Space Physics Research Laboratory

0 REPLIES 0