Skip to main content
Associate II
October 14, 2024
Solved

Write SD card using bluenrg 332ac

Hi,

I am trying to write the IQ data to the SD card (i.e., write the received CTE pkt to the SD card). However, I found that Bluenrg-332ac has a cortex M0 core, which may not be able to drive an SD card. Is it possible to use this cortex M0 core for SD card writing?

Thanks,

Jason

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
October 15, 2024

Sure, a Cortex-M0 can access an SD-Card - even 8051s, AVRs, et al can do it!

eg, 

http://elm-chan.org/fsw/ff/#:~:text=It%20can%20be%20incorporated%20into%20small%20microcontrollers%20with%20limited%20resource%2C%20such%20as%208051%2C%20PIC%2C%20AVR%2C%20ARM%2C%20Z80%2C%20RX%20and%20etc.%20Also%20Petit%20FatFs%20module%20for%20tiny%20microcontrollers%20is%20available%20here.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

3 replies

Andrew Neil
Andrew NeilBest answer
Super User
October 15, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
JasonYangAuthor
Associate II
October 15, 2024

Thanks Andrew! I also wanna ask can I use cubeMX to build programs for the Bluenrg-332ac chip?

Andrew Neil
Super User
October 15, 2024

@JasonYang wrote:

 can I use cubeMX to build programs for the Bluenrg-332ac chip?


 

"The BlueNRG-LP and BlueNRG-LPS lines have been rebranded as STM32WB06/07 and STM32WB05, now seamlessly integrated into the STM32Cube ecosystem"

https://www.facebook.com/watch/?v=1579234726355456

https://www.st.com/en/embedded-software/stsw-lp-profiles.html

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.