Skip to main content
Associate
April 28, 2025
Solved

VL53L8CX Power up sequence

  • April 28, 2025
  • 1 reply
  • 897 views

Hi John, 

Could please confirm if the slew rate requirement of VL53L8CX is satisfied in the EVM X-NUCLEO-53L8A1? 

Mukeshk_1-1745822684620.png

Mukeshk_0-1745822667610.png

 

We're considering to use TI's TLV751180330PDSQR to power up the VL53L8CX sensor. But the TLV751180330PDSQR supports 11mV/µS approx. Also, there is no graph where we can infer the O/P slew for the LDK130M33RY or LDK130M18R. 

Best answer by John E KVAM

It doesn't matter much how long it takes the power comes up. The MCU is not running until you download the firmware and issue the start command. The VCSEL power is not required until you issue the start command. 

The trick is just put capacitor or or use an LDO that does not come on extremely fast. 

All those parts will work just fine. 

- john

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
May 12, 2025

It doesn't matter much how long it takes the power comes up. The MCU is not running until you download the firmware and issue the start command. The VCSEL power is not required until you issue the start command. 

The trick is just put capacitor or or use an LDO that does not come on extremely fast. 

All those parts will work just fine. 

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.