cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1X-SATEL detailed datasheet for current and power consumption details

sreejithrnair2026
Associate II

Hi Team,

 

I could only find the databrief and not the datasheet for VL53L1X-SATEL breakout boards. Could you provide a detailed datasheet mentioning the current consumption and power consumption at 2.8V, 3.3V and 5V respectively?

I currently have a VL53L1X-SATEL breakout board for development and do you recommend the input voltage to be in 2.8V, 3.3V or 5V for this breakout board to obtain best performance from this sensor breakout board?

Looking forward to your immediate and esteemed response.

Best Regards

Sreejith R Nair

1 REPLY 1
Zhiyuan.Han
ST Employee

Hi

There is a LDO XC6222B281MR-R on the VL53L1X-SATEL breakout board, it used to covert different input voltage level to 2V8 output, so no matter which voltage supply you connected, finally the VL53L1X will only get 2V8 voltage, so the performance will be same no matter 2.8V, 3.3V or 5V. 

 

About the VL53L1X detail power consumption, please find it in page19 of datashee Datasheet - VL53L1X - A new generation, long distance ranging Time-of-Flight sensor based on ST's FlightSense technology

 

Br

Zhiyuan.Han


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.