cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1X outdoors

MWatt.2
Associate

The VL53L1X outdoor performance is hindered by huge amounts of noise, and wildly fluctuating results, compared to indoors. I notice that the demos I can find online about this sensor conveniently never show it outdoors, although some articles mention it being used as a reversing sensor, or even a drone landing sensor...

Also, since this is supposedly the official Q&A place for ST devices, why is there such a dearth of answers here? A previous query regarding this outdoor problem received no satisfactory answer.

I found somebody asking about a filter, only to be told it's not a visible light sensor anyway.

Is it me, or is this sensor not meant for outdoor use? I'm only a hobbyist roboticist, and the simple code I've written so far works superbly indoors, but point this sensor towards daylight and all bets (and readings) are off.

Am I missing a code setting, or is there actually a filter that will solve this issue. I know I'm repeating questions asked before, but the lack of definitive answers is frustrating.

Any suggestions?

Max

8 REPLIES 8
IMi��
Associate

No answer from ST?

John E KVAM
ST Employee

Sorry for the slow reply. This is entirely my fault. The email alerts were not getting to me.

But I should have checked anyway.

As you guessed, it's an indoor sensor. We didn't intend it that way, it's just physics.

The sensor outputs an eye-safe laser light. If you could see it, it would be about as bright as a common Red LED on must electronics.

Outdoors we go up against the sun. Which generates a ton of 940nm light. (Oddly, there is not as much 940nm as the visible frequencies, but still a lot.)

And all that light looks to the sensor like noise.

When the signal to noise ratio goes too low, we cannot get an answer.

The drone landing works because the sensor is pointed down - away from the sun.

You will also see the sensor works in the shade of a building.

But in sunlight, with any direct light we cannot give an answer.


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'
Khee .1
Associate

Hi, I am an embedded developer.

It was mentioned that it was used as a reverse sensor or even a drone landing sensor, so I immediately tested it with Aduino.

The result was failure.

Modifying parameters inside short and long modes does not work in external natural light.

"ambient light 200 kcps/SPAD = Short 1300mm" within the data sheet

There's this part, but this is an inside story of an office with sunlight outside the window.

John E KVAM
ST Employee

​It's a signal to noise problem. The eye-safe laser is only about as bright as an indicator LED. In sun-light the SPADs get saturated with the sunlight and simply cannot 'see' the signal.

The sensor's light is 940nm and thus invisible. But the sun generates a  huge amount of 940nm completely screwing up your results.

In modern buildings, low-e glass is used and that blocks an awful lot of non-visible light.

Your results show that your glass may be more toward the clear spectrum in the graph below.

(From https://www.efficientwindows.org/lowe.php)

We are looking at the issue, but the only solution appears to be a lot more SPADs (so they don't saturate). And of course that's expensive.

0690X00000BuffBQAR.jpg


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'
Piotr Roszak
Associate II

Hi,

I am trying to better understand the meaning of configuration registers in VL53l1x to mitigate some problems. Do you know if there is any reference manual for VL53l1x that has some more detailed information? Resources available on ST site seem to be lacking the information. E.g. it would be beneficial for me to understand meaning of the following registers:

PHASECAL_CONFIG__TIMEOUT_MACROP

RANGE_CONFIG__VCSEL_PERIOD_A

RANGE_CONFIG__VCSEL_PERIOD_B

RANGE_CONFIG__VALID_PHASE_HIGH

SD_CONFIG__WOI_SD0

SD_CONFIG__INITIAL_PHASE_SD0

Thank you.

Piotr

John E KVAM
ST Employee

​ST deliberately does not publish what this stuff does. Working at that level is a real pain - even we have trouble with it. Instead we published a couple of APIs. The APIs aren't amazingly easy to follow but they are tons better than dealing at the register level. The PERIOD A and B are the times between the small blasts of light. By making them shorter you get more 'pings' per millisecond, but you limit the range of the chip. So setting up for short, Medium and long  affect these registers. The reason that A != B is to prevent radar aliasing - which you can google.

  • john


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'

Thank you for the reply and your hints. I will try to understand what is the meaning of the registers.

Best,

Piotr

Fasaw.2
Associate

The use of TCXO in radio packages is for the tight on-frequency transmission, it narrows the general band which your radios occupy, and improves the receiver sensitivity because the transmitters are placing here with their energy where they're intended too, and the receiver is asking inside the right area