cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1 TOF sensor: We use the VL53L1CBV0FY/1 sensor. 1. What is the cleaning protocol if dust gets on to the sensor? 2. Is this sensor available with dark protective film to enable easy detection and removal of the same during use?

GRavi.1
Associate II

We have sensors failing because of what looks like dust or debris that is getting on the sensor.

Also, often it is difficult to detect and remove the Kapton tape covering the sensors. The tests we run pass even though the film has not been removed sometimes. This is a problem because there are performance issues later on that are easily fixed by removing the kapton tape.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
John E KVAM
ST Employee

A blast of air from one of those compressed air cans is the best way to do it.

We suggest a coverglass made of Acrylic, PMMA, Polycarbonate, or glass.

There is an article I wrote on this subject at the top of this community page.

I'd give that a read.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
GRavi.1
Associate II

Hi John,

Thanks for your reply to my question.

One of my questions was not clear. When we purchase the sensor, it comes with a clear protective Kapton film on it. Due to the fact that it is clear, it is difficult to detect by the naked eye or simple vision systems. Also, the sensors pass our functional tests with or without the Kapton tape. Do the sensors come with an opaque protective film instead of the clear kapton film? If not, is it possible for ST to create a variant with an opaque protective film as an option? The opaque film will be easier to detect during functional testing and we will not need to rely on the human eye.

Thanks

Gopal

John E KVAM
ST Employee

That tape is the only thing we could find that would survive the required 3 re-flows that the cellphone vendors demanded. There is nothing opaque that would do this and not leave a residue on the sensor. Sorry about that. I know it's a problem.

Imagine our dismay when a pre-production run of 100 cell-phones had to be dis-assembled because they left the tape on.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
GRavi.1
Associate II

Thanks John!