cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1X orientation and ROI

SBann.1
Associate II

Dear,

I want to implement a people counting algoritme using the VL53L1X ToF sensor. I want to build my own PCB for it. I found out that when the sensor is rotated by 90 degrees (gold filters in a row), the edges of a door are measured better then when I mount it straight (gold filters side by side). I'm using a ROI of 8x16.

Is there any explanation for that, or am I doing something wrong?

Thanks in advance.

Kind regards,

Stijn

1 REPLY 1
John E KVAM
ST Employee

I've seen an issue like this, but only with a coverglass. If the coverglass is not exactly parallel with the sensor, you can get some issues wiht symmetry.

But the light goes out in a symmetric cone, and unless you have a tilted coverglass you should get the same answers.

(I'm assuming when you rotated the sensor you switched from an 8x16 to a 16x8.)

Try the same experiment without the coverglass. Or use the crosstalk free glass that was included with the Eval kit. Does that work better?

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.