2024-08-23 9:35 AM
Hi,
I am looking to print only the signalrate in MCPS of the VL53L1. What should I do?
Solved! Go to Solution.
2024-08-26 7:41 AM
Do your range. When the range is complete, call:
2024-08-26 7:41 AM
Do your range. When the range is complete, call:
2024-08-26 7:56 AM
What is the difference between getsignarate and getsignalrateperspad could u please elaborate?
Thank you
2024-08-26 8:49 AM
We care about the total signal rate. We can use as little as 0.5M counts per second, but would really like to see 20M counts, and can deal with more - but it's a waste of power. So we alter the number of photon detectors we use. The SPAD (Single Photon Avalanche Diode) array is adjustable from 4 to 256. (Some SPADs are occluded, so it's not an integer number).
So a relatively dull target can return 20Mcounts with 216 SPADs and a bright target can return the same 20Mcounts but it does it by using only 15 SPADs.
If you want to compare the brightness of your targets you need to get Signal per SPAD. This is the only way to compare the reflectivity of your targets.
- john