2023-05-30 07:47 AM - last edited on 2023-08-08 04:53 AM by Anne BIGOT
Hello,
I'm trying to use the VD6283 sensor on a X-NUCLEO-6283A1 plugged in a Nucleo-64 STM32F401.
For this, I've installed the latest ST-Link drivers and the software STSW-IMG301. My board is well recognized on Windows device manager as a "STM STLink Virtual COM Port", but when I try to launch the VD6283_GUI application, I've the following error : "SensorSystem..ctor():Le format de la chaîne d'entrée est incorrect" / "SensorSystem..ctor():Input string is not in correct format".
I've tried to launch it also with admin privileges but it's still not working.
Application version : 1.0.0 - r862
Windows : 11 Pro
Thanks
2024-05-23 05:17 AM - edited 2024-05-23 05:17 AM
Hello,
Sorry for this really late answer.
A new GUI has just been release for the VD6283 within the STSW-IMG301 package.
It is version : 1.0.1