cancel
Showing results for 
Search instead for 
Did you mean: 

Values obtained with range status 2 and 7 are accurate or not?

Akansha
Associate II

Hi,

I am working on VL53L1X Sensor for designing obstacle detection sensor. When i am testing my sensor's range in office environment, it is showing range status 2 and 7 so frequently even at Timing Budget 140ms.

Distance between target and sensor is only 2m still it's showing fluctuations around 100cm.

Please tell me weather i should consider values obtained with range status 2 and 7 or not?

Regards and how to reduce fluctuations obtained.

Akansha

1 REPLY 1
John E KVAM
ST Employee

Both are warnings. You can choose to use them.

The user guide defines the errors as:

2 VL53L1_RANGESTATUS_SIGNAL_FAIL Raised if Signal value is below the internal defined threshold.

7 VL53L1_RANGESTATUS_WRAP_TARGET_FAIL Wrapped target, not matching phases.

So 2 - the number of photon are too few to get a good value. Its a warning telling you the result will not be very accurate.

7- A wrap fail indicates the sensor thinks the target if so far away that it appears near. (Google Radar Aliasing. It's interesting.) But you can get the 7 error with motion as well.

Again a warning. You can choose to use the range or not.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.