2023-10-08 1:02 AM
Vl53l3CX works well when i init it with DataInit and StartMeasurement Function,but when i add a OffsetCalibration to its init sequence,it output a distance of 8191 mm,which is obviously wrong .Paraments of calabration function are shown in the following picture,is there anything wrong.any advice will be appreciated.
Solved! Go to Solution.
2023-10-08 4:50 AM
the rangestatus of the first measurement is always 255,use VL53LX_ClearInterruptAndStartMeasurement function get
next normal measurement.
2023-10-08 4:50 AM
the rangestatus of the first measurement is always 255,use VL53LX_ClearInterruptAndStartMeasurement function get
next normal measurement.