cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple byte read for VL53L5CX?

KWine
Senior

We seem to be having trouble getting through the vl53l5cx_init(&Dev); function for the VL53L5CX. We can read single bytes but multiple byte (4) reads trigger the TIMEOUT and the ULD doesn't load successfully. Here is our RdMulti function:

uint8_t RdMulti(
        VL53L5CX_Platform *p_platform,
        uint16_t RegisterAddress,
        uint8_t *p_values,
        uint32_t size)
{
    uint8_t DeviceAddress = p_platform->address;
 
    Wire.beginTransmission(DeviceAddress);  
    Wire.write((RegisterAddress & 0xFF00) >> 8); //MSB
    Wire.write(RegisterAddress & 0x00FF); //LSB
 
    uint8_t status = Wire.endTransmission(false); 
    if (status) { // failed
        return status;
    }
 
    uint32_t i = 0;
    status = Wire.requestFrom(DeviceAddress, size);
    if(status != size){
    return 1; // failed
    }
 
    while (Wire.available()) {
        p_values[i++] = Wire.read();
    }
    
    return 0;
}

This is a pretty standard multiByte read function for Arduino so we are a bit surprised it doesn't work. There doesn't seem to be enough diagnostics to determine why not. Any ideas about what we might be missing? Any way to change the TIMEOUT?

Can you suggest a way for us to verify our I2C communications besides uint8_t error = vl53l5cx_is_alive(&Dev, &isAlive); which we successfully negotiate?

We have tried this at 100kHz and 400 kHz I2C bus speeds on multiple platforms with the same result. We have used a similar multiByte read function to successfully talk with dozens of I2C sensors including the VL6180X, VL53L0, and VL53L1. Not sure what we could be missing...Thanks for any suggestions you might offer.

1 ACCEPTED SOLUTION

Accepted Solutions
KWine
Senior

Just for completeness, we have this working with the Arduino IDE using this library now. We had to modify the usual multiple byte read/write functions to handle large variable byte sizes. Probably more than one way to manage this but what is in the repo works.

View solution in original post

3 REPLIES 3
John E KVAM
ST Employee

I'm going to bet that the Arduino has a limit to their multi-byte write.

The chip has no program in it when it boots. It's simply running a bootloader.

The Init function downloads some 80K of program.

So 'size' in the code is huge.

And the Arduinto might be limited to 128 or 256 bytes.

You might have to break the multi-byte write into chunks of 100 bytes or so.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
KWine
Senior

Thanks for the answer John. I did try to increase the buffer to 1024 bytes but the program hung; at least I didn't get an error!.

At 256 bytes I see the same behavior as with the 32 and 64 byte buffer sizes described above

I will try breaking the multi-read and write functions into smaller byte chunks...

KWine
Senior

Just for completeness, we have this working with the Arduino IDE using this library now. We had to modify the usual multiple byte read/write functions to handle large variable byte sizes. Probably more than one way to manage this but what is in the repo works.