cancel
Showing results for 
Search instead for 
Did you mean: 

IR080C0-IC09-A066-2 cover window for VL53L1X

Ali_SE
Associate

I am using cover glass window IR080C0-IC09-A066-2. I want the design to be IP69. Where I can get the information that the cover glass can withstand If it is subjected to high water pressure (10000 kPa) and high temperature(80*C)?

1 REPLY 1
Anne BIGOT
ST Employee

Hello,

The cover glasses are not certified against pressure nor temperature.

Some customers are using them up to 100 degrees and tested it at 1m underwater for 30 minutes but no test were done by ST.

Regards

Anne


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'