2024-11-26 11:47 PM - edited 2024-11-26 11:47 PM
Hi,
We have a board featuring 5 VL6180X sensors and I noticed some oddities regarding the initial offset and scale in the latest production run:
The initial offset appears to be roughly in spec with the datasheet (Table 18. Ranging specification), although we have quite a few sensors at the maximum offset (and in the datasheet this is after 3 reflow cycles, we only have 1).
The linearity is far worse than what I see in "Figure 6. Typical ranging performance".
The largest issue for us is the inability to measure below 15mm. Some sensors simply register 0mm (4 boards out of a batch of 30 had this issue).
I was wondering if this is the expected behavior of the sensors, or if we're doing something wrong in our design/production?
Regards,
Sytse
FYI, our design: