cancel
Showing results for 
Search instead for 
Did you mean: 

Initial accuracy of VL6180X (i.e. after reflow)

SytseReitsma
Visitor

Hi,

 

We have a board featuring 5 VL6180X sensors and I noticed some oddities regarding the initial offset and scale in the latest production run:

  • Some sensors are unable to measure any distance below 15mm
  • The ranging linearity between different sensors is +/- 10mm (taken as the delta between a 20mm and a 68mm measurement to a matte aluminium plate).
  • Initial offset is varying +/- 10mm

 

The initial offset appears to be roughly in spec with the datasheet (Table 18. Ranging specification), although we have quite a few sensors at the maximum offset (and in the datasheet this is after 3 reflow cycles, we only have 1).

The linearity is far worse than what I see in "Figure 6. Typical ranging performance".

The largest issue for us is the inability to measure below 15mm. Some sensors simply register 0mm (4 boards out of a batch of 30 had this issue).

I was wondering if this is the expected behavior of the sensors, or if we're doing something wrong in our design/production?

Regards,

Sytse

FYI, our design: 

SytseReitsma_0-1732693479806.png

 

0 REPLIES 0