2024-08-30 04:06 PM
I am trying to use the VL53L4CD as a low power tamper sensor so that it interrupts when someone removes a lid. I am using the ULP driver and I pulled in SetDetectionThresholds from the other driver. I have been able to configure it to interrupt whenever the lid is outside of a threshold range (in case the lid is smashed in or removed), which seems to do exactly what I want. However, if I quickly remove the lid completely so that the sensor detects nothing, it does not generate interrupts.
Is there a configuration that tells it to interrupt when it sees nothing?