2022-02-07 2:20 AM
Can this product VL53L0X work in high vaccum range condition( 10^-3 to 10^-8 torr)?
What is the resolution of this product VL53L0X?
What is working temperature range of this product VL53L0X?
Solved! Go to Solution.
2022-02-07 12:39 PM
The sensor has air in it. But there is a hole - otherwise it would explode during reflow. But the datasheet says a slow ramp up is required to allow time for the air pressure to escape.
So the vacuum is not the problem but a rapid change in air pressure would be.
The resolution is 1mm. However the accuracy is more like +/- 3%. And maybe +/- a 5mm below 2cm.
The working temperature is stated in the datasheet - -20 to +70 degrees C.
If you need higher temps and better short distance linearity, just wait. It's almost out.
2022-02-07 12:39 PM
The sensor has air in it. But there is a hole - otherwise it would explode during reflow. But the datasheet says a slow ramp up is required to allow time for the air pressure to escape.
So the vacuum is not the problem but a rapid change in air pressure would be.
The resolution is 1mm. However the accuracy is more like +/- 3%. And maybe +/- a 5mm below 2cm.
The working temperature is stated in the datasheet - -20 to +70 degrees C.
If you need higher temps and better short distance linearity, just wait. It's almost out.
2022-02-09 5:50 AM
Thank you @John E KVAM