Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL6180X Not working with 10KHz I2C Frequency

Dear members,I am currently trying to interface Arduino Atmega 328p with VL6180X via I2C Bus. I have prepared basic code for reading Range value in single shot and continuous mode, it is working file. Now I changed I2C SCL to 100 KHz, 50 KHz, 20 KHz ...

VL53L0X Header files

Hello I'm currently trying to create a driver for the mbed platform (especially the LPC1768, as I work with this one the most) and I wanted to know, if the following header files are actually needed:windows.htime.hSERIAL_COMMS.hAlso, are the log file...

VL53L01 optical center register setting

Hi.Please help me with VL53l1.1)     Is it possible to read distance from individual pixel or is it only some kind of interpolation of the 4 x 4 region?2)     Is there a description of registers which should be modified (and how they should be modifi...

baev_al by Associate III
  • 2011 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L0X I2C Commands

​Can someone point me in the direction where I can find a document giving the I2C register locations to control the VL53L0X. I am trying to read out ranges using an FPGA and the standard I2C bus but all I have found is the device address is 0x52.Than...

RNobe by Associate
  • 4381 Views
  • 3 replies
  • 0 kudos

How to improve color accuracy?

Hi all,I have been experimenting with the X-NUCLEO-53L1A1 and the NUCLEO-F401RE and here are my results. Actual distance White Box Black Box Difference20cm 20.4cm 19.4cm ...

VL6180X measurement in a tube (FoV change?)

We'd like to measure distance in a tube with VL6180X. Tests with a diameter of approx. 5 cm show that the max. distance is reduced and the sensor is underranging. That is probably because the sensor receives some light reflected from the side walls. ...

rastik by Associate III
  • 1734 Views
  • 2 replies
  • 0 kudos