Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X FOV not operating as per specification

Hi, We have been testing the VL53L1X for a while. The primary intend is to measure the occupation a container (30cmx30cmx80cm) filled by small objects (10cmx10cm). We would like to limit the number of sensors to have a low energy consumption (system ...

ALaga.1 by Associate
  • 1317 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L0X linearity observation

We are using VL53L0x for measuring piston position inside syringe.We consider piston position at bottom of syringe as reference position.As we move piston to top, the difference between actual and measured reading start increasing.At bottom differen...

YGude.1 by Associate II
  • 1358 Views
  • 1 replies
  • 0 kudos

Resolved! VL6180X unstable range results

Hi,Readings from my VL6180X sensor are very unstable. They vary about +-8 mm from measure to measure.I tried with Nucleo board and official api, and also with Arduino board and Sparkfun code. 2,8V power supply is from linear regulator, measured objec...

Resolved! How have best accuracy at short distances: VL6180 or VL6180X?

Hi!I notice that in the datasheet of both VL6180 and VL6180X, there is EXACTLY the same plot of distance measurement. So that's leaving me to the question: Who is best for short distances, VL6180 or VL6180X?Have a look at page 12/87 here:Proximity an...

DMårt by Lead
  • 3097 Views
  • 2 replies
  • 0 kudos

Resolved! Problem with multiple sensors (3) on the I2C bus and C++ API

Hi ST team and community !I'm here because i have some troubles on the processus of initialisation of multiple sensors VL53L1CB.I use the following library available on gitHub : https://github.com/stm32duino/VL53L1The processus is the following :Shut...

userLM by Associate
  • 1875 Views
  • 2 replies
  • 0 kudos