Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is VL53L0X_REG_RESULT_PEAK_SIGNAL_RATE_REF?

Range Status value 3 is "Min Range Fail", which is checked by reading from VL53L0X_REG_RESULT_PEAK_SIGNAL_RATE_REF.What is the Peak Signal Rate Ref.?​I'm finding how to differentiate between a reflective sheet and a high gloss stainless steel like a ...

WOh.2 by Associate II
  • 1838 Views
  • 2 replies
  • 1 kudos

Resolved! Is there a way to differentiate between reflective sheets and other reflective materials like mirrors with the VL53L0X?

As you know, the reflective sheet is very bright regardless of the reflective sheet surface angle.However other reflective materials, such as mirrors, are only bright when the surface angle is perpendicular to the VL53L0X.​In such cases, it is diffic...

WOh.2 by Associate II
  • 2246 Views
  • 3 replies
  • 1 kudos

Resolved! TOF sensors VL53 ranging limitations with ambient light

Hi. We are starting a new automation project that needs to detect distance to objects as small as 5 cm by 5 cm, at a distance from 5 cm up to 200 cm. I have been testing VL53L3CX, and VL53L1 through Satel eval. boards. Connected to a proprietary hard...

Example 10: Motion indicator example.

In the example file there is this comment.   /* (Optional) Change the min and max distance used to detect motions. The   * distance between min and max must never be >1500mm, otherwise the function below returns error 127       min value is 400 max v...

BBald.1 by Associate II
  • 1246 Views
  • 1 replies
  • 0 kudos

Having problems with VL53L0X controlling via stm32F103c8

Hello,I have a uni project which involves VL53L0X   ToF sensor, at first I thought it is easy I2C sensor, but when learning about it, found out that I was wrong . As I understood this sensor requires API to run it, but i cant find anywhere on the ...

DSimp.1 by Associate III
  • 1694 Views
  • 1 replies
  • 0 kudos