cancel
Showing results for 
Search instead for 
Did you mean: 

Teseo-LIV3F, no satellite position.

Sergei
Associate II

Hello, Can you help me?

I assembled a module on the Teseo-liv3f basis with a passive antenna (A25-4102920-AMT02). And I can not get the coordinates in nmea messages (screenshot in attach). What could be the problem?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
24 REPLIES 24
Francesco Virlinzi
ST Employee

Hi Sergei.

Do you have LNA and SAW filter in the RF-path?

Regards

Francesco

Sergei
Associate II

Francesco,

I do not have an LNA and SAW filter. I use a minimum of connections.

Thank you.

Francesco Virlinzi
ST Employee

​Hi Sergei.

Sorry for the wrong image. I'l take an action to fix the document.

LNA and SAW are strongly suggested as reported in Chapter '6'.

Sorry for the mistake.

Regards

 Francesco

Sergei
Associate II

Francesco,

quote "Chapter 6.1 A passive antenna can be directly connected to Teseo-LIV3F. Take care that the antenna has to be close to the module...."

What about this? It is also mistake?

Regards

Francesco Virlinzi
ST Employee

Hi Sergei

It seems you are reading an old doc version.

The new one is online @

Regards

Francesco

FResi
Associate II

Hi Francesco,

I have the same problem with my Teseo-LIV3F module. It is connected to an active GPS antenna with an external power supply.

I receive several GPS satelliteᅠ with a very good field strength as following picture:

0690X000006CK1UQAW.png

The first time I tested the module, I've got the fix 3D for about 4 hours. 

After that, I can't have the fix and I don't have the position:

0690X000006CK1ZQAW.png

I've tried to update the ephemeris but with no result

 0690X000006CK1eQAG.png

In all my tests, only one time I saw one GLONASS satellite for about half an hour.

Can you help me?

Best regards

Francesco

Francesco Virlinzi
ST Employee

Ciao Francesco

Is the module restarting correctly powering-OFF an ON?

Thanks

Regards

Francesco

FResi
Associate II

Ciao Francesco,

I turned it OFF and ON several time, while it was working (FIX 3D) and not working (no FIX).

I'm using Teseo-Suite Pro v5.2.3.1.

Every time I powered-OFF and ON, I could receive NMEA messages, write commands and receive several GPS satellite with good C/N.

Regards

Francesco

Francesco Virlinzi
ST Employee

Ciao Francesco

Could you check in which production slot has been assembled the module you have?

On top of the shield:

0690X000006CKN6QAO.png

"YWW" means 'Year-week'

Thanks

Ciao

Francesco