cancel
Showing results for 
Search instead for 
Did you mean: 

TESEO III accuracy

Gero
Associate II

Hi,

Doing randoms tests on the TESEO III accuracy, I've found an horizontal accuracy of 14m for 95% of the locations with extremes of 23m. Does ST have more informations about the TESEO III accuracy ? Are there tests that have been published ?

Thanks

Regards

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

I'm sure they have published CEP specs.

Your results do seem particularly awful, but I think that's on you and your antenna or RF side. Does not seem consistent with a properly executed test. When peopl​e generate spec numbers it is usually with very expensive and very well placed antennas to provide optimal results.

I've posted plots to this GNSS subforum.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

https://community.st.com/s/feed/0D50X00009ZEutBSAT

CEP99 well inside 5m, and the bulk of the hits well inside 2.5m

Make sure you don't have airflow over the IC or TCXO

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks !

Are you using SBAS ?

Francesco Virlinzi
ST Employee

Ciao

Teseo3 in the default configuration guarantees:

  • 1.5m CEP50 (this is public result in the DS)

and we are close to

  • 2m CEP90

I think there something strange in your platform.

SBAS is On by default in ST firmware.

Regards

Francesco