cancel
Showing results for 
Search instead for 
Did you mean: 

Taseo-LIV4F Firmware Upgrade for NavIC

jitusanwale
Associate II

While upgrading Taseo Firmware for NavIC through UART interface to PC, I got the following error message:

Upgrade command error
Please check software baud rate or select recovery mode


My setting are:
Loader baud rate: 115200
Software baud rate 115200

Jumper settings

J6:2-3 (FW-UPG)

J7: 2-3(FW-UPG)

J11: NC

Request to confirm the correct baud rates or how to upgrade the firmware.

2 REPLIES 2
liaifat85
Senior III

Check if both the loader baud rate and the software baud rate match, as they do in your settings (115200 in this case).

Thanks for your reply.

The problem is fixed now. Earlier, I was using 40 pin connector Rx and Tx pins which then I changed to J10 Rx and Tx.