2023-12-15 12:34 AM
Hello community users! There is a question that needs to be asked. Any help would be greatly appreciated! We want to know Can S2_LP UHF module receive the differential correction data generated by our own gnss base station? So we'd like to know the supported protocols as well as a description of the format. Can S2-LP support transparent protocol? We need to use the tuning method + baud rate + bandwidth that it supports.
2023-12-18 12:06 AM
Hi Eric
Sorry I don't know the S2_LP device.
This is a GNSS community covering Teseo GNSS product.
You cold try asking in the 'Interface and connectivity ICs' community.
Sorry
Regards
Francesco
2023-12-22 01:19 AM
...then asked in S2_LP UHF module PROTOCOL - STMicroelectronics Community