2021-12-23 8:23 AM
Hello.
My name is aoki
I am using Nucleo-F401RE and X-Nucleo-GNSS1A1.
TESEO-SUITE is no longer displaying anything at all.
I have tried the following to solve this problem.
A. I initialized the flash of Nucleo-F401RE and downloaded the sample software, but there was no change.
B. I reinstalled TESEO-SUITE, but there was no change.
C. When I check the serial communication with Tera Term, I can receive the data, but there is no longitude
and latitude information from the satellite.
From the above results, it is the internal flash of Teseo -LIV3F that is suspicious.
Please let me know how to restore the factory default settings for Teseo -LIV3F implemented in X-Nucleo-GNSS1A1.
Thank you
2022-06-17 6:15 AM
Hello,
what you could do is to restore the FW on the Teseo-LIV3F using the FWUPG java tool on your PC and the FW_Updater application on your NUCLEO-F401RE.
You can find both of them in the X-CUBE-GNSS1 package, respectively in folders Utilities\PC_Software\FirmwareUpdaterTool and Projects\NUCLEO-F401RE\Applications\FW_Updater.
Hence to start the firmware upgrading process you should:
BR
Silvio