cancel
Showing results for 
Search instead for 
Did you mean: 

My TESEO-LIV3F has stopped connecting to the Teseo-Suite! How can I restore factory settings?

Iyaku
Associate II
 
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
16 REPLIES 16
Francesco Virlinzi
ST Employee

Hi

Did you change anything in the firmware configuration?

Which tool are you using? EVB-LIV3F or X-Nucleo-GNSS?

Thanks

Regards

Francesco

Iyaku
Associate II

Yes, I tried to configure the firmware. But the process freezes and Teseo no longer communicates with the PC.

No I do not use VB-LIV3F or X-Nucleo-GNSS.

I have a Teseo module soldered to the board.

From your MCU-host you should perform a firmware-update where the configuration is removed.

You can take the firmware @ https://www.st.com/content/st_com/en/products/embedded-software/automotive-infotainment-and-telematics-software/teseo-liv3fsw.html

Take care that to perform firmware-update your MCU has to driver the Teseo-LIV3F.nReset pin.

Just a question: what were you configuring? may be it's just a baud-rate issue?

Did you see PPS blinking? May you can communicate with I2C port.

Regards

Francesco

Iyaku
Associate II

But can I complete firmware-update where the configuration is removed from the PC and terminal program or using any other program?

Iyaku
Associate II

speed did not change exactly

Worked only on UART, PPS is not possible to control.

Hi

Firmware update is always possible because internally it doesnt' care on the configuration.

On the PC:

  • you have to use the firmware update tool (in the Teseo-Suite);
  • in the firmware update tool you have to enable:
    • Recovery mode
    • Erase NVM
    • Baud 115200

On the board:

  • connect the UART
  • Push "Start" button in the firmware-update tool
  • Trigger the module reset (this is mandatory)

On Module reset the firmware update will start.

Hope this helps

Regards

Francesco

Hi

So that's the point, Teseo-Suite throws an error when you press the STA808x / 9x FW Upgrade button in the Tools menu?

0690X00000ArcnlQAB.jpg0690X00000ArcngQAB.jpg

Hi

Which version of Teseo-Suite are you using?

Did you install Teseo-Suite as Administrator?

You can try using the attached stand-alone version of firmware-update.

Rgards

Francesco

Hi

thanks for the help

version of Teseo-Suite - 5.2.3.4

install Teseo-Suite as Administrator