2020-07-30 8:50 AM
Is there IRNSS available or need any IC for IRNSS. if other require then how it communicate with STA8090FG.
2020-07-30 12:06 PM
Teseo III supposedly supports NAVIC/IRNSS
What you'd normally do is contact your local sales office, and have them provide you with specific data and support
https://www.ion.org/publications/abstract.cfm?articleID=16979
Quetel has a Teseo V based solution, but suspect that's on the more expensive side
https://www.quectel.com/infocenter/news/552.htm
I'd also imagine that the local government, and the program itself, can provide you with an extensive list of supported technology and partners.
Outside of India support is likely to be tepid.
2020-07-30 12:13 PM
Telit SL869T3-I is on a uBlox NEO form factor, uses a TESEO III, with an L5 down converter providing a 3rd RF down via external inputs.
https://www.telit.com/m2m-iot-products/positioning-timing-modules/positioning-gnss-sl869t3-i/
Ask your local ST sales contact for an L5 NAVIC reference design for the TESEO III
2020-07-30 10:46 PM
Hi
> Is there IRNSS available or need any IC for IRNSS. if other require then how it communicate with STA8090FG.
IRNSS constellation is supported on ST chips: STA8090FG + STA5635
STA5635 is an external RF-IC able to acquire L5.
Regards
Francesco
2020-11-06 8:36 PM
IRNSS constellation is supported on ST chips: STA8090FG + STA5635 . Pls. help to share commands to detect external antenna.