Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs products
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
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs products
STM32 MPUs Boards and hardware tools
STM32 MPUs Software development tools
STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
Microcontrollers
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
Pravin kumar
Associate II
since
2020-07-11
2023-06-14
User statistics
5
Posts
0
Solutions
0
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About Pravin kumar
Options
Report User
User Activity
Posts
Replies
I am using STM8S001J3 for PWM at TIMER 1 channel 4(PC4) PIN NO 7,but not getting pwm..pls.suggest.
2020-08-06
void PWM(void)//timer1 channel4{ TIM1_ARRH = 0x03; // Reload counter = 960TIM1_ARRL = 0xc0;TIM1_PSCRH|= 0; // Prescalar = 0 (i.e. 1)TIM1_PSCRL |= 0;//TIM1_CR1 = 0; // Up counter.TIM1_CR1|= 0; // Edge aligned counter.TIM1_RCR |= 0; /...
Is the GNSS IC STA8090FG suitable for IRNSS?
2020-07-30
Is there IRNSS available or need any IC for IRNSS. if other require then how it communicate with STA8090FG.
Re: Is the GNSS IC STA8090FG suitable for IRNSS?
2020-11-06
IRNSS constellation is supported on ST chips: STA8090FG + STA5635 . Pls. help to share commands to detect external antenna.
Re: I am using STM8S001J3 for PWM at TIMER 1 channel 4(PC4) PIN NO 7,but not getting pwm..pls.suggest.
2020-08-06
enable the clock for TIM1 in CLK_PCKEN register & Is the port output ;besic timer 4 is running at 4 ms interrupt.using stm8-so8-disco for debug.
Re: I am using STM8S001J3 for PWM at TIMER 1 channel 4(PC4) PIN NO 7,but not getting pwm..pls.suggest.
2020-08-06
Please share SPL libary for PWM on Timer 1 channel 4 for stm8s001j3