cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot enable the autonomous STAGPS engine on TESEO-LIV3R

MPete.5
Associate II

I have a Teseo LIV3R on a breakout board connected (via UART) to Tesio Suite. I'm trying to figure out how to enable STAGPS and test its functionality. Unfortunately I cannot enable the autonomous STAGPS engine using the command:

$PSTMSTAGPSONOFF,1

When sending the command $PSTMSTAGPSONOFF,1 to the module, I get no response. I would expect a response such as $PSTMPOLSTARTED. When sending the command $PSTMCFGAGPS,1 I get a response that the AGPS engine has been enabled. I would like to enable the autonomous STAGPS functionality though but I am not able to.

Hopefully someone canhelp or have an idea what the problem is?

Also, I was not able to confirm if the autonomous STAGPS function is enabled as default. Does anyone know if it is, and how to confirm this?

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Francesco Virlinzi
ST Employee

Hi

ST-AGPS is enabled by default in LIV3R.

Regards

Francesco

Thanks Francesco, do you know how I can verify that as well as switch on/off this feature?

I had no luck using $PSTMSTAGPSONOFF,1 and $PSTMSTAGPSONOFF,0

Thanks,

Martin.