GNSS positioning

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do i interpret 2D / 3D Acc. in Teseo-Suite Pro?

I have the Teseo-Liv3f eval kit and it finds 9 sats and i have 3D fix.  The lat/long/alt values are very stable but i cannot find any description of 2D and 3D Acc.  It seems the accuracy should be very "good" so what is the unit of these large number...

0690X000006CB8BQAW.png
TLubk by Associate II
  • 487 Views
  • 2 replies
  • 0 kudos

VCC_IO of Teseo LIV3F

Hello there!I'm about to decide on a GNSS module for my application. I'm curious about the VCC_IO in the datasheet. First it seems that the supply voltage of the module can be 2,1 to 4,3 V. However, the VCC_IO is demanded to be 3 to 3,6 V (in contras...

hendrik by Associate II
  • 588 Views
  • 3 replies
  • 0 kudos

www.st.com

FAQ on Teseo-LIV3FQ) Where can I find information on Teseo-LIV3FA) All the information are available on-line on www.st.com  Q) Which constellations are supported on Teseo-LIV3F?A) Teseo-LIV3F supports GPS, Glonass, Galileo, BeiDou and QZSS constellat...